ACTION#.SOURCEID

Description

Some action sources require a specific source ID number. For example, if your action source is a Digital Input, then a source ID of 1 would correspond to Digital Input 1.

The range of the source ID will depend on the value of the corresponding source. If the source is modified, the range and units of the source ID may change, and the source ID value will default to the first valid value.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Depends on ACTION#.SOURCE

Range

Depends on ACTION#.SOURCE
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
ACTION1.SOURCEID

3905h

01h

Unsigned8

-

-

Read/Write

No

ACTION2.SOURCEID

3905h

02h

Unsigned8

-

-

Read/Write

No

ACTION3.SOURCEID

3905h

03h

Unsigned8

-

-

Read/Write

No

ACTION4.SOURCEID

3905h

04h

Unsigned8

-

-

Read/Write

No

ACTION5.SOURCEID

3905h

05h

Unsigned8

-

-

Read/Write

No

ACTION6.SOURCEID

3905h

06h

Unsigned8

-

-

Read/Write

No

ACTION7.SOURCEID

3905h

07h

Unsigned8

-

-

Read/Write

No

ACTION8.SOURCEID

3905h

08h

Unsigned8

-

-

Read/Write

No

ACTION9.SOURCEID

3905h

09h

Unsigned8

-

-

Read/Write

No

ACTION10.SOURCEID

3905h

0ah

Unsigned8

-

-

Read/Write

No

ACTION11.SOURCEID

3905h

0bh

Unsigned8

-

-

Read/Write

No

ACTION12.SOURCEID

3905h

0ch

Unsigned8

-

-

Read/Write

No

ACTION13.SOURCEID

3905h

0dh

Unsigned8

-

-

Read/Write

No

ACTION14.SOURCEID

3905h

0eh

Unsigned8

-

-

Read/Write

No

ACTION15.SOURCEID

3905h

0fh

Unsigned8

-

-

Read/Write

No

ACTION16.SOURCEID

3905h

10h

Unsigned8

-

-

Read/Write

No

ACTION17.SOURCEID

3905h

11h

Unsigned8

-

-

Read/Write

No

ACTION18.SOURCEID

3905h

12h

Unsigned8

-

-

Read/Write

No

ACTION19.SOURCEID

3905h

13h

Unsigned8

-

-

Read/Write

No

ACTION20.SOURCEID

3905h

14h

Unsigned8

-

-

Read/Write

No

ACTION21.SOURCEID

3905h

15h

Unsigned8

-

-

Read/Write

No

ACTION22.SOURCEID

3905h

16h

Unsigned8

-

-

Read/Write

No

ACTION23.SOURCEID

3905h

17h

Unsigned8

-

-

Read/Write

No

ACTION24.SOURCEID

3905h

18h

Unsigned8

-

-

Read/Write

No

ACTION25.SOURCEID

3905h

19h

Unsigned8

-

-

Read/Write

No

ACTION26.SOURCEID

3905h

1ah

Unsigned8

-

-

Read/Write

No

ACTION27.SOURCEID

3905h

1bh

Unsigned8

-

-

Read/Write

No

ACTION28.SOURCEID

3905h

1ch

Unsigned8

-

-

Read/Write

No

ACTION29.SOURCEID

3905h

1dh

Unsigned8

-

-

Read/Write

No

ACTION30.SOURCEID

3905h

1eh

Unsigned8

-

-

Read/Write

No

ACTION31.SOURCEID

3905h

1fh

Unsigned8

-

-

Read/Write

No

ACTION32.SOURCEID

3905h

20h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

ACTION1.SOURCEID

40600

9E98

Unsigned8

Read/Write

-

ACTION2.SOURCEID

40601

9E99

Unsigned8

Read/Write

-

ACTION3.SOURCEID

40602

9E9A

Unsigned8

Read/Write

-

ACTION4.SOURCEID

40603

9E9B

Unsigned8

Read/Write

-

ACTION5.SOURCEID

40604

9E9C

Unsigned8

Read/Write

-

ACTION6.SOURCEID

40605

9E9D

Unsigned8

Read/Write

-

ACTION7.SOURCEID

40606

9E9E

Unsigned8

Read/Write

-

ACTION8.SOURCEID

40607

9E9F

Unsigned8

Read/Write

-

ACTION9.SOURCEID

40608

9EA0

Unsigned8

Read/Write

-

ACTION10.SOURCEID

40609

9EA1

Unsigned8

Read/Write

-

ACTION11.SOURCEID

40610

9EA2

Unsigned8

Read/Write

-

ACTION12.SOURCEID

40611

9EA3

Unsigned8

Read/Write

-

ACTION13.SOURCEID

40612

9EA4

Unsigned8

Read/Write

-

ACTION14.SOURCEID

40613

9EA5

Unsigned8

Read/Write

-

ACTION15.SOURCEID

40614

9EA6

Unsigned8

Read/Write

-

ACTION16.SOURCEID

40615

9EA7

Unsigned8

Read/Write

-

ACTION17.SOURCEID

40616

9EA8

Unsigned8

Read/Write

-

ACTION18.SOURCEID

40617

9EA9

Unsigned8

Read/Write

-

ACTION19.SOURCEID

40618

9EAA

Unsigned8

Read/Write

-

ACTION20.SOURCEID

40619

9EAB

Unsigned8

Read/Write

-

ACTION21.SOURCEID

40620

9EAC

Unsigned8

Read/Write

-

ACTION22.SOURCEID

40621

9EAD

Unsigned8

Read/Write

-

ACTION23.SOURCEID

40622

9EAE

Unsigned8

Read/Write

-

ACTION24.SOURCEID

40623

9EAF

Unsigned8

Read/Write

-

ACTION25.SOURCEID

40624

9EB0

Unsigned8

Read/Write

-

ACTION26.SOURCEID

40625

9EB1

Unsigned8

Read/Write

-

ACTION27.SOURCEID

40626

9EB2

Unsigned8

Read/Write

-

ACTION28.SOURCEID

40627

9EB3

Unsigned8

Read/Write

-

ACTION29.SOURCEID

40628

9EB4

Unsigned8

Read/Write

-

ACTION30.SOURCEID

40629

9EB5

Unsigned8

Read/Write

-

ACTION31.SOURCEID

40630

9EB6

Unsigned8

Read/Write

-

ACTION32.SOURCEID

40631

9EB7

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

ACTION1.SOURCEID

40600

Unsigned8

Read/Write

-

ACTION2.SOURCEID

40601

Unsigned8

Read/Write

-

ACTION3.SOURCEID

40602

Unsigned8

Read/Write

-

ACTION4.SOURCEID

40603

Unsigned8

Read/Write

-

ACTION5.SOURCEID

40604

Unsigned8

Read/Write

-

ACTION6.SOURCEID

40605

Unsigned8

Read/Write

-

ACTION7.SOURCEID

40606

Unsigned8

Read/Write

-

ACTION8.SOURCEID

40607

Unsigned8

Read/Write

-

ACTION9.SOURCEID

40608

Unsigned8

Read/Write

-

ACTION10.SOURCEID

40609

Unsigned8

Read/Write

-

ACTION11.SOURCEID

40610

Unsigned8

Read/Write

-

ACTION12.SOURCEID

40611

Unsigned8

Read/Write

-

ACTION13.SOURCEID

40612

Unsigned8

Read/Write

-

ACTION14.SOURCEID

40613

Unsigned8

Read/Write

-

ACTION15.SOURCEID

40614

Unsigned8

Read/Write

-

ACTION16.SOURCEID

40615

Unsigned8

Read/Write

-

ACTION17.SOURCEID

40616

Unsigned8

Read/Write

-

ACTION18.SOURCEID

40617

Unsigned8

Read/Write

-

ACTION19.SOURCEID

40618

Unsigned8

Read/Write

-

ACTION20.SOURCEID

40619

Unsigned8

Read/Write

-

ACTION21.SOURCEID

40620

Unsigned8

Read/Write

-

ACTION22.SOURCEID

40621

Unsigned8

Read/Write

-

ACTION23.SOURCEID

40622

Unsigned8

Read/Write

-

ACTION24.SOURCEID

40623

Unsigned8

Read/Write

-

ACTION25.SOURCEID

40624

Unsigned8

Read/Write

-

ACTION26.SOURCEID

40625

Unsigned8

Read/Write

-

ACTION27.SOURCEID

40626

Unsigned8

Read/Write

-

ACTION28.SOURCEID

40627

Unsigned8

Read/Write

-

ACTION29.SOURCEID

40628

Unsigned8

Read/Write

-

ACTION30.SOURCEID

40629

Unsigned8

Read/Write

-

ACTION31.SOURCEID

40630

Unsigned8

Read/Write

-

ACTION32.SOURCEID

40631

Unsigned8

Read/Write

-